FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > How to use built-in high-speed counters
FAQ
How to use built-in high-speed counters
I would like to know how to use built-in high-speed counters.
Answer
For contacts to drive the coils of high-speed counters, use the contacts which are normally on during high-speed counting.
Do not use the input (X000 to X007) of the high-speed counters as contacts to drive the output coils (OUT) of the high-speed counters.
Do not use the input (X000 to X007) of the high-speed counters as contacts to drive the output coils (OUT) of the high-speed counters.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- High-speed Counting
- Series
- MELSEC-F series