FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Keyword protection of the MELSEC-F series
FAQ
Keyword protection of the MELSEC-F series
I have registered a keyword for protecting the MELSEC-F series. How I can forcibly reset the protection if I forget the keyword?
Answer
The keyword protection cannot be forcibly reset.
Since only the keyword that has been registered by the user is acceptable, please take measures to ensure the keyword is not lost.
If deleting data does not cause any problem, all programs and parameters including the keyword setting, can be cleared by executing the clear PLC memory function from the peripheral connected.
If deleting data does not cause any problem, all programs and parameters including the keyword setting, can be cleared by executing the clear PLC memory function from the peripheral connected.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series
May I have your opinion?
Related FAQ
- Distinguishing the usage of standard counters and high-speed counters
- Scan time while operation of a programmable controller CPU is being monitored using GX Works2
- Deleting all programs and data from the memory
- Turning on a bit in the data register
- Using the FX3U-ENET-ADP and the RS-232C/RS-485 together (FX3U/FX3UC series)