FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Accessing the FX3U-ENET-ADP Ethernet communication special adapter at remote locations from GX Works2 via Internet
FAQ
Accessing the FX3U-ENET-ADP Ethernet communication special adapter at remote locations from GX Works2 via Internet
Is it possible to access the FX3U-ENET-ADP at overseas or domestic locations from GX Works2 via Internet?
Answer
Using the VPN (Virtual Private Network)*1 connection service enables the communications.
VPN is a technology that connects networks by encrypting the communication contents.
(*1: A VPN connection service support partner will help you build a VPN system.)
VPN is a technology that connects networks by encrypting the communication contents.
(*1: A VPN connection service support partner will help you build a VPN system.)
- Product Name
- MELSEC-F Series
- Product Category
- FX3G,FX3GC,FX3U,FX3UC
- Series
- Network/Communication
May I have your opinion?
Related FAQ
- Assignment of input/output numbers (MELSEC-F series)
- FX series products that support CC-Link Ver.2.0
- Number of FX3U-ENET-L Ethernet interface blocks that can be connected to the FX3U series
- MELSOFT connection of the FX3U-ENET-L Ethernet interface block
- Connection of the FX3GC series and FX3U-ENET-ADP