FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Parameter setting of FX3U-1PG
FAQ
Parameter setting of FX3U-1PG
When setting parameters, such as maximum speed and pulse rate, in the FX3U-1PG, there are two types of parameters. Which parameter will be used?
Answer
Whether the positioning parameter is used or the extension positioning parameter is used can be selected in BFM#32 (positioning parameter selection). Select BFM#0 to #15 for K0 and select BFM#33 to #52 for K1. * When the parameter in BFM#32 is changed during operation, this change becomes valid from the next operation.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Operation speed change during a positioning operation of the FX3U-1PG
- Pulse output system of the FX3U-1PG pulse output block
- Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
- Thickness of ground wire