FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
FAQ
Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
How many personal computers can be communicated with the FX3U-ENET-L simultaneously?
Answer
For communications using MELSOFT connection, such as GX Developer, GX Works2, GOT1000, and MX Component, up to two personal computers can be used.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U, FX3UC
- Series
- Network/Communication
May I have your opinion?
Related FAQ
- MELSOFT connection of the FX3U-ENET-L Ethernet interface block
- Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
- AnyWire-compatible master block of the FX programmable controller
- Terminal layout of the FX3U-1PG and FX2N-1PG pulse output blocks
- Adding two channels of the RS-232C port in the FX3G series