FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Adding two channels of the RS-232C port in the FX3G series
FAQ
Adding two channels of the RS-232C port in the FX3G series
I would like to add two channels of the RS-232C port in the FX3G series. How can I add the communication expansion boards and adapters?
- Category :
Answer
Select the 40-point or 60-point type FX3G series main unit. In this case, two FX3G-232-BDs can be connected. When FX3G-CNV-ADP is used, an FX3U-232ADP can be used instead of an FX3G-232-BD.
- Product Name
- MELSEC-F Series
- Product Category
- FX3G
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
- Communication format setting
- Parameter setting of FX3U-1PG
- Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3UC series
- Operation speed change during a positioning operation of the FX3U-1PG