FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Number of GOTs (GOT1000 series) that can be connected to a FX3U-ENET-L
FAQ
Number of GOTs (GOT1000 series) that can be connected to a FX3U-ENET-L
How many GOTs (GOT1000 series), such as GT14, GT15, and GT16, can be connected to a FX3U-ENET-L?
Answer
Up to two GOTs can be connected to a FX3U-ENET-L and MELSOFT connection needs to be set.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U, FX3UC
- Series
- Network/Communication
May I have your opinion?
Related FAQ
- Target address change during the positioning operation in the FX3U-1PG
- E-mail sending/receiving function of the FX3U-ENET-L
- Using the FX3U-16CCL-M and FX2N-16CCL-M together
- Number of FX3U-16CCL-M CC-Link master blocks that can be connected to the FX3U series
- Number of FX3U-ENET-L Ethernet interface blocks that can be connected to the FX3U series