FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Programmable controller series which the FX3U-1PG pulse output block can be added to
FAQ
Programmable controller series which the FX3U-1PG pulse output block can be added to
On which programmable controller series, can FX3U-1PG be added to?
Answer
FX3U/FX3UC series (Ver. 2.20 or later)
* To connect the FX3U-1PG to the FX3UC series, the FX2NC-CNV-IF connector conversion adapter or the FX3UC-1PS-5V extension power supply unit is required.
* To connect the FX3U-1PG to the FX3UC series, the FX2NC-CNV-IF connector conversion adapter or the FX3UC-1PS-5V extension power supply unit is required.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Terminal layout of the FX3U-1PG and FX2N-1PG pulse output blocks
- Positioning blocks/module that can be connected with a manual pulse generator
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
- Target address change during the positioning operation in the FX3U-1PG
- File format that can be saved to a CF card in the FX3U-CF-ADP