FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Connection of the FX3G series and the FX3U-ENET-ADP
FAQ
Connection of the FX3G series and the FX3U-ENET-ADP
Is optional equipment required for connecting the FX3G series and the FX3U-ENET-ADP?
- Category :
Answer
An FX3G-CNV-ADP is required.
* When the FX3U-ENET-ADP is used with other special adapters, connect the FX3U-ENET-ADP at the last stage (left end).
* When the FX3U-ENET-ADP is used with other special adapters, connect the FX3U-ENET-ADP at the last stage (left end).
- Product Name
- MELSEC-F
- Product Category
- FX3G
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Connection of expansion boards and a memory cassette to the FX3G series main unit
- Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2
- Using a fixed latched (battery backed) type device as a general type device
- Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3U series
- E-mail sending/receiving function of the FX3U-ENET-L