FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Using the FX3U-16CCL-M and FX2N-16CCL-M together
FAQ
Using the FX3U-16CCL-M and FX2N-16CCL-M together
Is it possible to add the FX3U-16CCL-M and FX2N-16CCL-M together to one main unit?
Answer
No, they cannot be added together. Only one FX3U-16CCL-M can be connected to one main unit. Multiple FX2N-16CCL-Ms can be connected to one main unit (depending on the programmable controller series and the number of other special extension units).
- Product Name
- MELSEC-F Series
- Product Category
- FX3G,FX3GC,FX3U,FX3UC
- Series
- Network/Communication
May I have your opinion?
Related FAQ
- Number of remote device stations that can be connected to FX2N-16CCL-M
- Connection of the FX3G series and the FX3U-ENET-ADP
- Connection of the FX3G series and the GT1020/GT1030 series (5 V type)
- MELSOFT connection of the FX3U-ENET-ADP Ethernet communication special adapter
- Number of FX3U-64CCL interface blocks that can be added to a main unit