FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Terminal layout on the output side of the FX3U-16MR/ES
FAQ
Terminal layout on the output side of the FX3U-16MR/ES
Are output side terminals of the FX3U-16MR/ES independent commons?
- Category :
Answer
Yes, they are independent common terminals.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Connection of expansion boards and a memory cassette to the FX3G series main unit
- Triac output type main units in the FX3 series
- Adding FX3U series expansion boards to an FX3UC series main unit
- Connection of the FX3G series and the FX3U-ENET-ADP
- Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2