FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3GC series
FAQ
Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3GC series
How many FX3U-ENET-ADPs can be connected to the FX3GC series?
Answer
One FX3U-ENET-ADP can be connected at the last stage (left end) of adapters for the FX3GC series.
* The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel (CH).
* The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel (CH).
- Product Name
- MELSEC-F Series
- Product Category
- FX3GC
- Series
- Main Unit, Network/Communication
May I have your opinion?
Related FAQ
- Connectors for FX3UC series
- Connection of the FX3G series and the GT1020/GT1030 series (5 V type)
- Station number setting in the "PLC System(2)" tab of PLC Parameter setting on GX Developer when non-protocol communication is performed
- Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3UC series
- Using the FX3U-16CCL-M and FX2N-16CCL-M together