FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
FAQ
Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
Which versions of the FX3U/FX3UC series main units support the function for accessing the other station of CC-Link using the FX3U-16CCL-M?
Answer
The main units with Ver.3.10 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices. (GX Works2 with Ver.1.73B or later is applicable.)
- Product Name
- MELSEC-F Series
- Product Category
- FX3U, FX3UC
- Series
- Main Unit, Network/Communication
May I have your opinion?
Related FAQ
- Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
- Connection of the FX3GC series and FX3U-ENET-ADP
- Operation of the first special function unit/block in the FX3UC series
- Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
- Model of the cable provided with the FX2N series extension unit