FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Electronic bypass function
FAQ
Electronic bypass function
When the electronic bypass function is used, can the MRS signal (operation enable/disable selection) be normally closed contact by changing Pr.17 (MRS input selection) to "2"?
- Category :
Answer
No, it cannot be normally closed contact. When the electronic bypass function is used, the setting of Pr.17 is disabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700