Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22293
  • Release Date : 2018/08/30 13:55
  • Update : 2023/02/13 15:31
  • Print

Regarding a mismatch found in the monitoring function of GX Works3

A mismatch was found between the actual operation of the PLC and the monitor status of GX Works3.
Is there a solution to fix the mismatch?
Category : 

Answer

Perform "Rebuild All" and initialize the memory before writing to the PLC.
"Rebuild All" converts the entire project and "Convert" only coverts the modified part of the program.
For further details please refer to GX Works3 Operating Manual.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Engineering Software
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries