Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22295
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the type of Ethernet connection cable

Which type of Ethernet connection cable should be used to connect FX5 CPU module and GX Works3(Computer)?
Category : 

Answer

Ethernet standard-compatible cable, category 5 or higher (STP cable) can be used.
*Straight cable can be used.
When connecting directly to the computer, cross cable can also be used.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?