Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22297
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the range of latch devices

From which to which number is the range of latch device(Power failure retention area)?
Can the link register (W) and file register (R) be latched?
Category : 

Answer

The latch range can be set arbitrarily by the customer.
The settings can be found in the memory/device settings of CPU parameters.
To back up the link register (W) and file register (R) devices, a battery FX3U-32BL (option) is required.
Product Name
FX5U, FX5UC
Product Category
CPU Module
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?