Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22300
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the maximum number of controllable axes of the bulit-in positioning function

What is the maximum number of the axes that can be controlled with the built-in positioning function of FX5 CPU module?
Category : 

Answer

Up to 4 axes can be controlled. Please use a transistor output type CPU module.
(By adding a high speed pulse input/output module,
maximum 12 axes (CPU built-in 4 axes+expansion 2 axes×4 modules) can be configured.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Simple Motion/Positioning Control Control
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?