Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22306
  • Release Date : 2018/08/30 13:55
  • Print

Regarding CW/CCW(Forward pulse/Reverse pulse) output of the built-in positioning function

Does CPU built-in positioning function support CW/CCW(Forward pulse/Reverse pulse) output?
Category : 

Answer

Yes, CW/CCW outputs are supported.
Up to 2 axes can be controlled by setting parameter from GX Works3.
Also, by adding high speed pulse input/output module, up to 8 axes can be added.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Simple Motion/Positioning Control
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?