Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22307
  • Release Date : 2018/08/30 13:55
  • Update : 2023/06/23 10:25
  • Print

Regarding I/O assignment on the module configuration diagram of GX Works3

Is it possible to check the I/O assignment of CPU or I/O extension modules on module configuration diagram of GX Works3?
Category : 

Answer

While the module configuration window is being displayed,
the I/O assignment can be checked by selecting the following options from the menu bar:
[Edit]→[XY Assignment Display]
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, I/O Module, Engineering Software
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries