FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Output frequency of the FX3U-1PG pulse output block
FAQ
Output frequency of the FX3U-1PG pulse output block
How much is the pulse output frequency of the pulse output block FX3U-1PG?
Answer
It is from 1 Hz to 200 kHz.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Programmable controller series which the FX3U-1PG pulse output block can be added to
- Changing the JOG speed in the FX3U-20SSC-H
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
- Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
- Number of FX3U-1PG pulse output blocks that can be connected to the FX3U/FX3UC main unit