Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 39274
  • Release Date : 2023/01/12 16:45
  • Print

Regarding the Connected/Disconnected Module Detection button on FX5-CCLGN-MS

Even if you click the Connected/Disconnected Module Detection button displayed on the "CC-Link IE TSN Network Configuration" setting screen, an error occurs and detection is not possible. Is there a solution?
Category : 

Answer

For the Connected/Disconnected Module Detection of FX5-CCLGN-MS, the network configuration of the subsequent stages can not be automatically detected unless the network has been established between the FX5-CCLGN-MS operating as the master station with at least one local or remote station.
Use the above function after establishing communication between FX5-CCLGN-MS with one or more local or remote stations.
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries