FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding program execution using SD Memory Cards
FAQ
Regarding program execution using SD Memory Cards
Is it possible to execute programs from an SD memory card installed in the FX5 CPU module?
Answer
It's possible. Use the boot operation function of the SD memory card.
*To use the boot operation function with the FX5S CPU module, you need to install an additional SD memory card unit: FX5-SDCD.
*To use the boot operation function with the FX5S CPU module, you need to install an additional SD memory card unit: FX5-SDCD.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Option
- Series
- MELSEC iQ-F Series