Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 39338
  • Release Date : 2023/02/14 17:29
  • Print

Regarding the requirement of SD Memory Card module function of FX5S CPU module

Does the FX5S CPU unit have any functions that require an SD memory card module: FX5-SDCD?
Category : 

Answer

SD Memory Card Module: FX5-SDCD is required for the following functions.
・Firmware update function ※ 1
・Memory card function (SD memory card forced stop, boot operation)
・Data logging function
・Memory dump function
・Backup/Restore
・File transfer function (FTP server)
・File transfer function (FTP client)
・Web server functions (user web pages)
※1 The firmware of FX5S CPU module can be updated using engineering tool. By updating the firmware from the engineering tool, it is possible to update the firmware without using the SD memory card module or SD memory card.
Product Name
FX5S
Product Category
CPU Module, Option
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries