FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the differences between Latches (1) and (2)
FAQ
Regarding the differences between Latches (1) and (2)
What is the difference between latches (1) and (2) on FX5U/FX5UC,FX5S CPU module?
Answer
Whether or not the latch range is set by default and the range to "clear values" from CPU memory operations are different.
You can clear with two options: clear only the latch (1) or clear latch (1) + latch (2).
You can clear with two options: clear only the latch (1) or clear latch (1) + latch (2).
- Product Name
- FX5U, FX5UC, FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series