FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding parameter setting for FX5-CCL-MS
FAQ
Regarding parameter setting for FX5-CCL-MS
Is it possible to set the FX5-CCL-MS parameters programmatically?
Answer
It is possible to set the basic/application settings in a program by selecting the parameter setting method to "Program."
Even if set by "program" is selected, "Station type," "Mode," "Station number" and "Transmission speed" must be set by parameter.
For program examples, see the following manual.
MELSEC iQ-F FX5 User's Manual (CC-Link)
Even if set by "program" is selected, "Station type," "Mode," "Station number" and "Transmission speed" must be set by parameter.
For program examples, see the following manual.
MELSEC iQ-F FX5 User's Manual (CC-Link)
- Product Name
- FX5-CCL-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series