FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication > Regarding Email function Attachments
FAQ
Regarding Email function Attachments
What are the file formats and file sizes that can be attached by the email function?
Answer
The file formats and file sizes that can be attached by the email function are as follows:
・Attachments: Up to one file
・File formats: Binary, ASCII, CSV
・File size: 32768 bytes
・Attachments: Up to one file
・File formats: Binary, ASCII, CSV
・File size: 32768 bytes
*The attached data must be generated by a program. Therefore, files (such as logging data) in the CPU module or SD memory card can not be attached.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series