FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding Bus Conversion Module Differences
FAQ
Regarding Bus Conversion Module Differences
There are two types of bus conversion modules, FX5-CNV-BUS and FX5-CNV-BUSC. What is the difference?
Answer
The FX5-CNV-BUS is an additional cable type.
・Used when the FX5-CNV-BUS previous module is an expansion cable type module.
・Used when the FX5-CNV-BUS previous module is an expansion cable type module.
The FX5-CNV-BUSC is an additional connector type.
・Used when the first module of the FX5-CNV-BUSC is an additional connector type module.
・Used when the first module of the FX5-CNV-BUSC is an additional connector type module.
- Product Name
- FX5U,FX5UC
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series