Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22304
  • Release Date : 2018/08/30 13:55
  • Print

Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3

Can the FX3 intelligent modules be selected on the module configuration diagram on GX Works3?
Category : 

Answer

As the parameter settings of the FX3 intelligent function modules are not supported by GX Works3,
they cannot be selected from the element selection window.
Please use the configure using the program.
Also, regarding the setting and programming , please refer to the corresponding manual of each FX3 intelligent function modules.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Engineering Software, GX Works3
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?