Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20815
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800/FR-F800

The P3 terminal is added depending on the capacity. Is it possible to connect the brake unit or brake resistor with both P/+ and P3?
Category : 

Answer

When connecting to the P/+, the current flows in the inrush circuit at the regenerative driving. This regenerative current may generate losses in the inrush circuit, which causes the overheat and damage of the inverter. Thus, connect the brake unit or brake resistor to the P3 terminal when the P3 terminal is prepared.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?