Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20835
  • Release Date : 2018/08/22 16:24
  • Print

Leakage current of the FR-BIF

In the Instruction Manual, it is described that the leakage current at the star connection is 4 mA. How much is the leakage current at the delta connection?
Category : 

Answer

For the 200 V type, the leakage current at the delta connection is 5 mA. For the 400 V type, it is 10 mA.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?