FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800-R2R
FAQ
FR-A800-R2R
When the winding diameter calculation is the thickness method and the normal speed control is performed, how can I set the initial speed to 20 Hz and the end speed to 40 Hz?
- Category :
Answer
They cannot be set with the frequency. Because the command is input at the line speed, consider the line speed of the initial winding diameter at 20 Hz. The frequency at the winding ending is determined by the result of the winding diameter calculation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-R2R