FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800
FAQ
FR-A800
When tuning the SF-V5RU by Pr.71 = 33, does the tuning result change between Pr.9 = 0 and Pr.9 = Rated motor current setting?
- Category :
Answer
Yes. When Pr.9 = 0, turning is performed with the inverter rated current.
Always set the rated motor current.
Always set the rated motor current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800