Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20901
  • Release Date : 2018/08/22 16:24
  • Print

Terminal 2 input selector switch when the PTC thermistor is connected

Does the DIP switch of the second terminal of the PTC thermistor (10 to 2 terminals) operate normally even after it is switched from V to I?
Category : 

Answer

When the DIP switch is changed to I, it does not operate normally because the internal resistance changes.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?