FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Monitoring function of the FR-A800-R2R
FAQ
Monitoring function of the FR-A800-R2R
Can the monitoring function of the terminal 1 input voltage and the terminal 1 after calibration (%) be monitored when Pr.363 is other than "5"?
- Category :
Answer
No, they cannot be monitored when Pr.363 is other than "5". They are enabled only when Pr.363 = 5.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus