FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A8NC/FR-A8AX
FAQ
FR-A8NC/FR-A8AX
Can I set the frequency from the CC-Link and FR-A8AX?
- Category :
Answer
The frequency setting in the communication cannot be used together with FR-A8AX. The priority of the FR-A8AX is equal to the second terminal analog input and it is enabled in the following operation mode. External operation mode, External/PU combined operation mode 2 (Pr.79 = 4), NET operation mode (Pr.339 = 1)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option