Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20922
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-GF

Can the same options as the FR-A800 be used for the FR-A800-GF?
Category : 

Answer

Yes, the options are the same as the FR-A800 standard model. Note that two options can be added at maximum. (One option is already used as standard.) Other communication options are unavailable.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?