FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Difference in the monitor function
FAQ
Difference in the monitor function
The motor torque and the torque monitor (power driving/regenerative driving polarity switching) are the monitor function of the 800 series. What is the difference between them?
- Category :
Answer
The same value is displayed in the initial setting. When negative output is enabled by setting "0" to Pr.290 (Monitor negative output selection), there are following differences. Motor torque: Displays positive values at forward power driving or reverse regenerative driving, and negative values for reverse power driving or forward regenerative driving. Torque monitor: Displays positive values at power driving and negative values at regenerative driving regardless of the rotation direction.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800