FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Anti-sway control
FAQ
Anti-sway control
When a swinging frequency is set in Pr.1074, do the setting values in Pr.1077 to Pr.1079 affect the control?
- Category :
Answer
No, it does not affect the control. When a swinging frequency is set in Pr.1074, the setting values in Pr.1077 to Pr.1079 are not referred. When Pr.1074 is set to "9999", the setting values in Pr.1077 to Pr. 1079 are referred.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800