FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800
FAQ
FR-A800
What is the "maximum output frequency" of the frequency accuracy in the common specification: "Within ± 0.2% of the maximum output frequency"?
- Category :
Answer
It is based on the maximum value that can be set for frequency. Specifically, it is 400 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800