Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21007
  • Release Date : 2018/08/22 16:25
  • Print

FR Configurator2

When editing the USB memory parameter copy file, the CP1 file is specified and edited. Can I generate a new CP1 file and transfer it to the inverter without using the existing CP1 file?
Category : 

Answer

Only the parameter setting values (USB memory parameter copy file: CP1 file) read from the inverter to USB memory can be edited. Customers cannot generate a CP1 file.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?