FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Frequency setting increment
FAQ
Frequency setting increment
When the setting frequency increments and monitor increments are set to 0.1 rpm with Pr.811 = 1, why is the value displayed in 1 rpm increments after monitoring?
- Category :
Answer
The value is displayed in 0.1 rpm increments under Vector control. However, the value is rounded down to the first decimal place and displayed in 1 rpm increments under other control methods.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800