FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > EMC filter (SF1306)
FAQ
EMC filter (SF1306)
An insertion type is employed for the terminal block. How can I insert the wire?
- Category :
Answer
There are two holes at the bottom of the EMC filter. The bigger hole at the lower part is for wire. Put the screwdriver into the small hole at the upper part and pull it up using the power of leverage to open the valve inside the hole used for wiring.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- SF1306