FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > PLC function
FAQ
PLC function
When changing the value of SD1144 (Set frequency writing (RAM)) with Y24 (Set frequency writing command (RAM)) ON to change the frequency using the PLC function, why does the frequency not change?
- Category :
Answer
The setting is enabled at the Y24 start-up. The frequency cannot be changed when Y24 is always ON. Turn ON Y24 when writing a frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800