FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Sine wave filter
FAQ
Sine wave filter
When using Real sensorless vector control, can I use the sine wave filter?
- Category :
Answer
The sine wave filter can be applied only under V/F control. When Pr.72 PWM frequency selection is set to 25, V/F control is set automatically. The applicable output frequency is 60 Hz or less.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- FR-A800, FR-A700