Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21080
  • Release Date : 2018/08/22 16:25
  • Print

SW1DND-FRC2 (FR Configurator2)

The communication error (ES:0x010a4001) occurs in Developer although the communication of FR Configurator2 can be performed. What are the possible causes for this?
Category : 

Answer

Check the setting value of Pr.414 (PLC function operation selection) and if the initial value: 0 (PLC function disabled) is set, set "1" or "2" and enable the PLC function.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR-A800, FR-F800, option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?