FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > FR-A800
FAQ
FR-A800
Is the installation compatible with the A500(L) series? FR-A520(L)-0.4K to 90K, FR-A540(L)-0.4K to 280K, FR-A540L-375K and 450K
- Category :
Answer
- The installation size is compatible for the following capacities.
Compatible: 200 V class 90K or lower, 400 V class 7.5K or lower and 18.5K to 280K- The installation size is compatible for the following capacities by using the optional intercompatib
Compatible: 200 V class 90K or lower, 400 V class 7.5K or lower and 18.5K to 280K- The installation size is compatible for the following capacities by using the optional intercompatib
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800