FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > DC reactor
FAQ
DC reactor
A DC reactor is not enclosed. Is no DC reactor required if harmonics are suppressed by other means than inverter reactors?
- Category :
Answer
If using an inverter with capacity of 75K or higher, or motor with capacity of 75 kW or higher, always select and install the inverter based on the capacity of the motor with DC reactor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800