Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21123
  • Release Date : 2018/08/22 16:26
  • Print

Multi-speed setting

When Pr.24 (4 speed) of multi-speed setting is only set and RH, RM, RL are all turned ON, which frequency is applied for the operation?
Category : 

Answer

If Pr 27 is not set, the operation starts at the speed of RL.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?