FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Reverse rotation prevention selection
FAQ
Reverse rotation prevention selection
When the reverse rotation is disabled by Pr.78 = 1 and rotation direction at restart is enabled by Pr.299 = 1, does the inverter perform reverse operation?
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
Yes, it does. When the inverter is coasting in the reverse direction, it starts in the reverse direction and switches to the forward rotation after a deceleration stop.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ